1/10/2020 10:24 AM | |
Joined: 7/28/2016 Last visit: 6/10/2024 Posts: 4 Rating: (0) |
Hello! I want to use a Simatic PG on our Mobile Machine at Mines. In this machine we have impedance grounded (IT system).The neutral of our 240V system is connected to grounding bus of the electrical panel which is further connected to clients grounding system situated miles away from the mine pit through trailing cable and then through overhead line.But as per Siemens Datasheet this device intended for operation on grounded power supply system.So if we use this Simatic PG in this condition will it effect the longevity or the warranty of this device? Thanks in advance. Shambo Attachmentfield_pg_m6_quick_install_guide_de_en.pdf (706 Downloads) |
Follow us on