3/17/2020 11:24 AM | |
Joined: 8/25/2006 Last visit: 9/19/2024 Posts: 2209 Rating: (278) |
Hello. CPU551 does not have integrated DP or PN interface, so there is no GSD for this CPU. What do you want to do with CPU551? Which CP do you use, CP50M0 or CP50M1? If you want to configure TDC (CP50M0) as a slave on DP network you should use GSD of Simadyn D SS52, for CP50M1 look at example. |
This contribution was helpful to2 thankful Users |
3/27/2020 6:03 AM | |
Joined: 8/25/2006 Last visit: 9/19/2024 Posts: 2209 Rating: (278)
|
Hello. Do you have D7-SYS installed as suggested here? For Step 7 V5.5 SP4 you will need D7-SYS V8.1. |
Follow us on