9/17/2019 3:16 PM | |
Posts: 1 Rating: (0) |
I was needing a GSD siemens S7300 for using in Sycon.net. I was trying communicate with Cifx using the Sycon.net in mode Slave. |
9/17/2019 3:31 PM | |
Joined: 9/27/2006 Last visit: 9/24/2024 Posts: 12282 Rating: (2685) |
Hello Ferreira; First, here is a link to the Simatic CPUs gsd files, select your model of CPU for the project to download the correct file: https://support.industry.siemens.com/cs/ww/en/view/113652 Next, the formulation of your question is not clear. You would need a S7-300 gsd file if the S7-300 CPU is to be used as a Profibus slave, your Cifx being the master. But you say you want to use the Cifx in slave mode? Actually, from the Hilscher site, the Cifx-50-DP is only a PC interface card for Profibus, the master would be whatever software uses the interface as a DP master (Sycon is the configuration software for the Profinbus network; the master is the PLC or SCADA program that is marked as master in the Sycin file).. Please describe your application with more details, maybe a diagram would help, so we may make sure you can configure the elements of your ^project correctly. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on