6/26/2016 10:40 PM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076) |
Please upload the file. |
6/26/2016 11:08 PM | |
Posts: 10 Rating: (0) |
AttachmentWEL (2).zip (325 Downloads) |
6/27/2016 10:41 AM | |
Joined: 10/7/2005 Last visit: 5/8/2024 Posts: 3004 Rating: (1046) |
For what it is worth, I fully agree with ixo65 and will also state that the file "Sequence.AWL" is an STL source file. In fact, it appear to be a complete S7 project source file as it contains UDT's, DB's, OB's, FC's and FB's. As such, the answer to Mark_pro's question "I have the file ending .AWL I would like to know which software could open it" is also already correctly provided by ixo65. |
Cheers |
|
This contribution was helpful to3 thankful Users |
Follow us on