11/5/2012 11:09 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello, Wincc v7.0 sp3 I want to create a comment function for operator->when alarm is coming in, operator has to acknowledge with comment. Comment with original alarm time+status+messagenumber is put into MSG_RTDATA_INSTANCECOMMENT_STRUCT. A archive alarm is then generated where a user text block is filled with data from MSG_RTDATA_INSTANCECOMMENT_STRUCT . The problem is that it doesn't work. 1 or two times it has worked all of the sudden... My apdiag shows this: Button OK klicked UserComment : sfs UserComment Selected Msg was acknowledged 0005-11-2012 10:58:04.56877168 / 2002 / Gemiddelde temperatuur ba Message with comment created The second last line is the data send to the comment_struct. This has to show in a user text block, but it is not working... it doesn't show up in the user text block... What can I do about this? The strange thing: I put in a printf function to see if something happend. Only added the line and all of the sudden it worked. After deleting the line, it didn;t work anymore and after trying again it did't work either.... The project was upgraded from 6.2 to 7.0 without running project editor... |
Last edited by: Oreca at: 11/5/2012 11:19 AMLast edited by: Oreca at: 11/5/2012 11:10 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on