7/3/2019 1:26 PM | |
Posts: 1 Rating: (0) |
Please help me i am facing problem in my machine last week my machine was working after power failure when i start the machine there is one error is showing on hmi 120202waiting for nc/plc connection and on NCU unit seven segmat indicate 3 instead 6 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/04/2019 10:18:31New subject after splitting |
|
7/4/2019 1:42 PM | |
Posts: 672 Rating: (56) |
Hi, Search on this site for the error message. There are probably 100 posts covering it. Pee |
7/4/2019 4:27 PM | |
Posts: 112 Rating: (11) |
Dear Shubi, our technical documentation on web says the following: 120202 Waiting for a connection to the NC/PLC Definitions: The operator panel is connected to the NC and PLC via a serial bus. This alarm occurs if the MMC is started for the first time and the NC/PLC ramp-up is not yet finished or the communication to these components is faulty. In connection with this alarm, all display values connected with the NC/PLC become invalid. Such faults are normal while the controls are ramping up (e.g. after resetting). Reaction: Alarm display. Remedy: The alarm disappears automatically as soon as the fault situation has ended. If this alarm is continuously present, a wide variety of faults may be the cause. (e.g. wire breakage, NC/PLC not ramped up, faulty address/data transfer rate configuration of one of the bus nodes, etc.). I would recommend you to contact the Siemens Hotline in that case: https://support.industry.siemens.com/my/ww/en/requests#createRequest you can see this post with the name of APC-Tech or Sir Nulizhang posts you can fimd gd solution |
Last edited by: Shafay at: 07/04/2019 16:30:13Last edited by: Shafay at: 07/04/2019 16:30:44 |
|
Follow us on