1/4/2012 6:23 AM | |
Posts: 11 Rating: (0) |
Dear Experts, In one of our project we are using Ultrasonic Open Channel Flow-Meter (Qty- 120) of siemens at remote locations. These flowmeters are HART based protocol. Using GSM/GPRS RTU Module, we are fetching data on GPRS from different filed locations in WinCC. 'PLEASE FIND ATTACHED FILE, IT SHOWS WHOLE STRUCTURE OF OUR SYSTEM' My doubt is who to fetch/collect all these parameters from remote locations into WinCC?? What & How should i do setting into the WinCC? Regards, mandar Attachmentsystem_architecture.pdf (69 Downloads) |
1/4/2012 10:14 AM | |
Posts: 1776 Rating: (95)
|
Hi, for your purpose you can use the Modbus TCPIP channel in WinCC. This channel is available in WinCC V7.0. Detailed informations are given in the WinCC Information system chapter: communication > Modbus TCPIP also have a look at this entry as an example http://support.automation.siemens.com/WW/view/en/37885119 |
1/4/2012 11:46 AM | |
Posts: 11 Rating: (0) |
thk u v much sir................... regards, mandar |
Follow us on