3/2/2020 8:00 AM | |
Posts: 31 Rating: (0) |
Quick question, how do I enable the S7 protocol on my Siemens 12CE PLC? |
3/2/2020 1:24 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
It is the same procedure as for S7 protocol, just select Modbus server instead of S7 server. See attachment for the addressing, because the Siemens informations are not complete. Select Modbus client in your Raspberry. For data logs it is logical, that the Logo serves the data and the Raspberry is the client and loading the data as needed. Depend on the first address of your client for coils or registers select 0 or 1 in the excel sheet for the start address. Regards, Scorp AttachmentModbus Tabelle 0_1.zip (453 Downloads) |
Last edited by: Scorp at: 03/02/2020 13:26:46 |
|
Follow us on