7/19/2017 9:32 AM | |
Joined: 3/14/2010 Last visit: 4/14/2024 Posts: 359 Rating: (5) |
Hi, schufri ! Thank you very much !!! I will try. |
9/1/2017 11:27 AM | |
Joined: 3/14/2010 Last visit: 4/14/2024 Posts: 359 Rating: (5) |
I have Win7 & WinCC v.7.0 +SP3+Upd1. I want to set up my WinCC project in order to unlock/lock Windows key combinations when WinCC RT is running according this https://support.industry.siemens.com/cs/document/332356/with-windows-server-2000-2003-windows-2000-professional-windows-xp-professional-and-windows-vista-what-should-you-do-if-disabling-the-key-combinations-is-ineffective-in-wincc-?dti=0&lc=en-WW See point 2“How can you have event-triggered disabling/enabling of Windows key combinations at Runtime?” But I think I can’t begin to make necessary settings until I have passed point 1 successfully, because "Check whether the following entries are present: In point 1 “1. What should you do if disabling the key combinations is ineffective in WinCC?” there is: "Table 01 ………….. Search for the code: HKEY_LOCAL_MACHINE/Software/Microsoft/Windows NT/Current Version/Winlogon The entrie GinaDLL = "almxgina.dll" is absent on my PC. NEXT The entrie “Userinit» is not like this : Userinit = "userinit,ALMXPMGR.EXE,nddeagnt.exe" as necessary, but like this : Userinit = C:\Windows\system32\userini.exe What to do ? May I correct the registry as necessary or not ? |
Last edited by: Alex3110 at: 9/1/2017 11:31:32 AMLast edited by: Alex3110 at: 9/4/2017 7:31:40 AM |
|
Follow us on