1/20/2017 2:50 PM | |
Joined: 4/28/2015 Last visit: 6/27/2024 Posts: 2 Rating: (1) |
Hi I would like to know how to use a usb serial converter with the iot2020 . I can send data with minicom but node-red cannot access /dev/ttyUSB0 . if i want to access the com port from the command line I get " /dev/ttyUSB0: Permission denied " . Can somebody point me in the right direction please . ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/20/2017 3:27:21 PMNew subject after splitting |
|
2/2/2017 11:34 AM | |
Posts: 5 Rating: (0) |
Yes, exactly that problem. I'll wait for the new example image. Thank you very much Mark |
2/27/2017 1:44 PM | |
Posts: 5 Rating: (0) |
Hi, do anyone have news on the New SD Example Image with Updated Node-red and Serial Ports working? Thanks in advance Mark |
6/3/2017 9:27 AM | |
Posts: 25 Rating: (1) |
I am also not able to see the USB PORTS with the image version 2.1.3. |
6/30/2017 10:21 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by sure94 is split to a separate thread with the subject How to communicate with the Modbus serial node? . Best regards |
8/3/2017 2:11 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by AutoGen_5750863 is split to a separate thread with the subject USB device in the IoT2040 often can't recongized by PC, what can do?. Best regards |
Follow us on