4/9/2020 4:59 PM | |
Posts: 6 Rating: (0) |
Hi all i'm asking help to understand how and if it's possible to use the function _writeRecord and _readRecord regarding the identification and maintenance data of the electronic plate I&M0. i've found the header and the struct inside the SIMATIC NET manual and i've created the same structure in the program, i've also copyed the procedure descripted in the online help (it's described the procedure to get the SINAMICS drive data set nr.47 but i think the mechanism is the same) but in no way i can get the function works... is there something that is missing? someone have ever tryed to do so with simotion via user program? in my case the return error is 16#FFFF_80A3. i'm using TIA portal V15 and Scout Fw5.2 the hardware tha i'm trying to access is: 6ES7 151-3BA23-0AB0 with 5 input module, 1 output module, 2 power module. attached the code thank for any help AttachmentuserProgram.txt (134 Downloads) |
4/17/2020 2:35 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Hello, please find behind attached Link the example about reading the module-information https://support.industry.siemens.com/cs/ww/en/view/53705461
|
With best regards, |
|
Follow us on