12/6/2016 10:33 AM | |
Posts: 6 Rating: (0) |
Yes, problem solved. Thank you. |
Last edited by: Nathan_South_Wales at: 12/6/2016 11:53:04 AM |
|
12/6/2016 12:14 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello Nathan, I have created a sample-picture with five tags and VB-scripts. To test it, you need to create the five tags ("counter_1"..."counter_5"). For the I/O-Fields the default "Update Cycle" is 2s, this should be changed to "Upon change". The script for incrementing the tags is in the picture, if the picture is not always displayed, you need to place it in a Global Action. Regards Georg Berghof AttachmentNewPdl1.zip (277 Downloads) |
PS: If this post did really help you, you may use the Rate-button |
|
12/15/2016 9:14 AM | |
Posts: 6 Rating: (0) |
Thank you for your support. The problem has been solved thankfully due to the assistance I've received from you both. |
Follow us on