3/19/2012 5:35 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi anuchisa, 1) To install the datamonitor server components on the WinCC client is a good idea. But pay attention to the network security: http://support.automation.siemens.com/WW/view/en/50203404 2) The license is ok so far, but offers acces for only 1 client simultaneously. However, if there is need, you can upgrade later on. The license has to be installed at the WinCC client (where the DataMonitor-Server is also installed). 3) It depends, what you like to do with the web client computer. If you only need "Webcenter" und "Trends and Alarms" on the DataMonitor Client, you do not need to install any additional software. For the"Process Screens", you must install a ThinClient (OCX). This can be done by browsing the DataMonitor-Server via Internet-Explorer, or can be directly installed from the installation DVD. |
mfG / Best regards |
|
Follow us on