5/11/2011 8:07 AM | |
Posts: 799 Rating: (42)
|
HI Jasner,
This is the plc address! You have tu ensure, that you can ping the cpu from the computer. So at first I would recomment you to ensure, that the ip address of the pc is in the same logical network as your PLC. (For this topic you can see this faq. Read the capital: IP-Addressing) When the ping from pc to plc is successful, everything should work fine.(If you don't know the ping command, you will also find description in the faq i postet above) best regards |
5/11/2011 11:22 PM | |
Posts: 10 Rating: (4) |
It is a wincc V7 screenshot David |
Follow us on