7/10/2018 2:11 PM | |
Posts: 3 Rating: (0) |
We would like to know if there is a list of supported USB sticks. We tried to connect my Siemens IOT2040 with a Huawey E173 and failed. Wr even followed the configuration instructions on oFono (listed bellow). We are using the Yocto 2.4.3 version that has a pre-installed oFono 1.20.
By following the steps presented we had two different outcomes.
Is there a guide to follow to connect the 3g modem using oFono? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/10/2018 3:04:31 PMNew subject after splitting |
|
7/11/2018 7:44 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, I haven't checked out Yocto 2.4.3 yet, but for our Example Image V2.2 (based on Yocto 2.2) there is an example how to connect a 3G mPCIe card and using ppp for configuring it. I think this could work with USB sticks as well. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
7/11/2018 2:28 PM | |
Posts: 3 Rating: (0) |
AutoGen_2256447, as you requested the outputs of the commands you asked us to do and the logs are attached. The outputs of the oFono commands are presented bellow: root@iot2000:~# killall ofonod root@iot2000:~# rm -rf /var/lib/ofono/* root@iot2000:~# /usr/lib/ofono/test/enable-modem Connecting modem /huawei_0... root@iot2000:~# /usr/lib/ofono/test/online-modem Setting modem /huawei_0 online... root@iot2000:~# /usr/lib/ofono/test/set-roaming-allowed Setting /huawei_0 to RoamingAllowed=1 root@iot2000:~# /usr/lib/ofono/test/enable-gprs Connecting modem /huawei_0... root@iot2000:~# /usr/lib/ofono/test/create-internet-context "XXXXX" "XXXX" "XXXXXX" Found context /huawei_0/context1 Setting APN to XXXXX Setting username to XXXXX Setting password to XXXXX root@iot2000:~# root@iot2000:~# /usr/lib/ofono/test/activate-context As said before when the connection is established it is lost few minutes later. We also realized that we are able to connect using the command “iot2000setup” and following the configuration steps of the menu. By doing this we get the same results as the command lines. We also realized that the first time the modem is connected it gets the name “huawei_0” and after losing connection it returns as “huawei_1”, what seems to make the whole configuration process necessary again. Attachmentlogscommandsoutputs.zip (207 Downloads) |
7/11/2018 2:50 PM | |
Posts: 3 Rating: (0) |
Bergmanu, thanks for the answer, we will evaluate the possibilities of using a mPCIe modem and test the installation steps of the manual. Regards |
Follow us on