5/13/2020 8:04 AM | |
Posts: 83 Rating: (0) |
Hi, In my FC program as shown below L DB9.DBB 18 I understand that it transfer the content of DB to local variable 1 and 0. But I did not see how local variable was called or used in THAT function program.?? And is there any difference with using TEMP variable instead of Local variable? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/13/2020 09:12:48New subject after splitting |
|
5/13/2020 9:34 AM | |
Joined: 3/30/2020 Last visit: 4/26/2024 Posts: 4453 Rating: (929) |
There is a technique that you transfer data to a local byte / word and then use the local bits in the program. What is assigned in the first two bytes of the temporary storage of the code block? Perhaps there are bits assigned? For example let us say the code looked like:
You may find later in the code (example):
|
Last edited by: qwazee at: 05/13/2020 09:37:20Last edited by: qwazee at: 05/13/2020 09:38:09Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
5/15/2020 3:04 AM | |
Posts: 83 Rating: (0) |
any iinput will be appreciated.. |
5/15/2020 6:43 AM | |
Posts: 83 Rating: (0) |
Hi Haiti, If it's not too much to ask, can you write comment for each code of line (see above my post). Tks |
Follow us on