6/4/2016 6:13 PM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33827 Rating: (4204)
|
Logo! Soft Comfort V8.0.0 is the latest version. Older versions are no longer sold by Siemens. |
6/8/2016 2:44 PM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33827 Rating: (4204)
|
If you only work with a 0BA6 (and younger), there is a solution in which you no longer need to use the interface selection. I have Windows 7. In my home directory (C: \ "username"), there is a directory ".LOGOComfort8.0". In this directory there is a file called "application.ini". Select at last the cable and the right COM Interface and close LOGO! Soft Comfort. Now open the file "application.ini" with Notepad and search for the contact: Change the entry in ConfirmBeforeComm = false and save the file. Now the cable and the corresponding end of COM interface is permanently selected. If you want to return to the normal interface selection, you need to move only Change back in ConfirmBeforeComm = true .
AttachmentApplication.ini.pdf (436 Downloads) |
Last edited by: ixo65 at: 6/8/2016 2:47:55 PMattachment Last edited by: ixo65 at: 6/8/2016 4:14:51 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on