10/9/2019 8:25 AM | |
Posts: 19 Rating: (0) |
I commissioned MasterDrive 6SE7022 for learning purpose and want to run a motor from drive locally with hardwired input. Kindly suggest me how to give analog input to drive and how to vary the speed accordingly. I jumped X101 (1) with X102 (19) to give command but it did not run Also inform if need to change any parameter accordingly. send an email if possible {snip} ------------------------------------------------------------------------------------------ |
Last edited by: mosi_0333 at: 10/09/2019 08:26:39Last edited by: The Helping Hand at: 10/09/2019 10:06:28Please only share personal contact information over personal messages. Last edited by: The Helping Hand at: 10/09/2019 10:07:12New subject after splitting |
|
10/9/2019 8:52 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please download & refer SIMOVERT MASTERDRIVES, MOTION CONTROL, COMPENDIUM manual. |
10/9/2019 10:22 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please refer attached sheet & wire up DI to activate StART, STOP, RELEASE signals. Also user need to apply variable analog input voltage signal so that motor speed can be varied. Please set the appropriate parameters correctly,Compendium Motion Control (MC 1.66) |
Follow us on