10/9/2019 8:32 AM | |
Posts: 19 Rating: (0) |
I commissioned MasterDrive 6SE7022 for learning purpose and want to run a motor from drive locally with hardwired input. I select P368 to 1 and p100 to 1, and drive shows 009 after cpmmissioning on display Kindly suggest me how to give analog input to drive and how to vary the speed accordingly. I jumped X101 (1) with X102 (19) to give command but it did not run Also inform if need to change any parameter accordingly. send an email if possible {snip} ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/09/2019 10:29:08Please only share contact information over personal messages. Last edited by: The Helping Hand at: 10/09/2019 10:30:45New subject after splitting |
|
10/9/2019 10:31 AM | |
Joined: 8/21/2014 Last visit: 4/18/2024 Posts: 949 Rating: (13) |
Closed because question was posted twice. Please use: MasterDrive 6SE7022: how to give analog input to drive? |
My Forum is the place to personalize your profile, |
|
Follow us on