5/2/2020 2:53 AM | |
Joined: 3/24/2018 Last visit: 11/1/2023 Posts: 236 Rating: (1) |
Hi, I migrated a project from MP277 Touch 10 inch "Wincc flexible 2008 SP2 into TP1200 12 inch "Advanced TIA V11 SP2" 1-After migration it appears an error in the TIA program for an IO Field"OBJECT_274" invalid visibility parameter. I noticed that: negative value in char data type not accepted in TIA program and I do not know the reason . When changing this value into positive,it is accepted by TIA program. Although this field is accepted in the Wincc flexible 2008 with the same parameter. 2- Also it appears a warning about the scripts. 3- Warning about: All the tags with the Char data type modified into Byte in the TIA program. 1 error and 2 warnings Please have a look at the attached file . How to solve these problems? Thank you in advance. Good bye AttachmentMigration.zip (71 Downloads) |
Last edited by: Pepsi Cola at: 05/02/2020 03:37:10Last edited by: Pepsi Cola at: 05/02/2020 11:23:07 |
|
Follow us on