7/5/2015 6:58 PM | |
Joined: 5/20/2015 Last visit: 4/24/2024 Posts: 216 Rating: (3) |
HEY DEAR ALL, FIRST OF ALL I WOULD LIKE TO THANKS CHRISTOP FOR HELP PREVIOUSLY, I AM HAPPY BY OPERATING MM440 OVER PROFIBUS DP USING FC14 ONLY, I CAN CONTROL AND MONITER ONLY ACT. OUT FREQUENCY. BUT I AM NOT FULLY SATISFIED BECAUS I WANT TO READ SOME ELECTRICAL PARAMETERS, LIKE ACT. OUT CURRENT, TORQUE, PF, ETC,. I AM TRYING TO GET OVER BUT ITS NOT WORKING, SO PLEASE ANYBODY OF YOU HELP ME? HERE I HAVE SHARED ALL THE NECESSARY DATA AND S7 PROJECT FILE, PLEASE GO THROUGH IT AND GUIDE ME AN EXACT PROCEDURE, ASAP. THANK YOU.
---------------------------------------------------------------------------------------------------- AttachmentMM440_SAMPLE.zip (454 Downloads) |
Last edited by: Min_Moderator at: 7/6/2015 2:46:08 PMNew subject after splitting Let's do it... |
|
7/7/2015 6:01 AM | |
Joined: 5/20/2015 Last visit: 4/24/2024 Posts: 216 Rating: (3) |
@ste39 i apolzie for mistake regarding sfc block, and thanks a lot for the help link, have a great day. |
Let's do it... |
|
7/8/2015 4:56 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello gabbar, Read carefully this FAQ: Operating Instructions: MICROMASTER PROFIBUS Optional Board Read carefully this thread: Accessing Micromaster 440 Parameters on S7 PLC ... - Siemens MICROMASTER 420 control by Profibus - Entries - Forum ... - Siemens MICROMASTER 420 control by Profibus via PPO1 ... - Siemens
|
7/9/2015 11:25 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello gabbar, I found this FAQ which also has a project (download under "Code") saves the project, Retrieve and then you will find a function block FB 63 with different DB. If you have Protool open MP 370 Touch, on the page MM4 Parameter, you will find the values that you need as you said above, go to the tags and you will find in which DB are associated the values. I hope help you MICROMASTER 4: Function block to operate on Profibus DP - ID ...
|
8/3/2020 4:51 PM | |
Joined: 12/28/2016 Last visit: 4/20/2024 Posts: 429 Rating: (44) |
this is help full for this solution https://support.industry.siemens.com/cs/ww/en/view/29157692 g120
|
Last edited by: Jen_Moderator at: 08/04/2020 08:33:27Optimized link. https://pnap.ir |
|
Follow us on