3/2/2021 11:12 AM | |
Joined: 8/12/2016 Last visit: 4/18/2024 Posts: 101 Rating: (3) |
Dear bg2429, I am trying to use the same concept by rather than playing a sound, i want a msgbox to showup. I created a global vbscript and on a tagchange value a msgbox shown with the username ( used the internal tags @CurrentUser) But when the tag is change, the msgbox in only shown on the basic wincc project (on the server) with no username. Is there a solution to do this ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/02/2021 13:35:42New subject after splitting |
|
3/2/2021 2:29 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello msgsadek, the using of the Windows Messagebox is in general no See the following FAQ for an alternative: https://support.industry.siemens.com/cs/ww/en/view/268859 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on