6/10/2020 10:40 AM | |
Posts: 8 Rating: (0) |
Dear All, I want to transfer data from Computer Based HMI via VB Scripts. To do that I have found an example from Siemens which is given as PDF. But, in this PDF example has explained with WinCC Flexible. So, my question is: Can I also do such project like this, with TIA Portal WinCC RA? Here you can find the PDF: PDF Waiting for your replies! Thank you. Attachment24677043_wincc_flexible_sql_datenbank_en.pdf (196 Downloads) |
6/10/2020 11:35 AM | |
Joined: 2/5/2013 Last visit: 9/21/2024 Posts: 321 Rating: (74) |
Hi, Below links may be helpful to you. How do you access an SQL database in WinCC Runtime Advanced using a script? How do you archive tags and messages in an SQL database with WinCC (TIA Portal) Advanced? |
Last edited by: Jen_Moderator at: 06/10/2020 12:31:56Optimized links. Please rate it. |
|
6/10/2020 12:26 PM | |
Posts: 8 Rating: (0) |
Dear Amol, Thank you for links! Have a nice day. |
6/10/2020 12:50 PM | |
Posts: 8 Rating: (0) |
Dear Amol, I'm just checking the links you have sent, and something has put me in a doubt. Could you please help? In second link I'm reading the PDF file and there it says: The following compenents must be installed on the PC.
My question is, can any computer without WinCC V15 reach the datas from SQL Server? Also, what I understood. PC system, which will be used for automation system shoud exist MS SQL Server 2014 and MS SQL Server Management Studio 17. Am I right? For example, PC system will be in the production area and my manager wants to check datas from sql server which he has not Computer with WinCC V15. Thank you! |
Follow us on