2/10/2020 10:01 AM | |
Joined: 1/7/2019 Last visit: 12/1/2020 Posts: 3 Rating: (0) |
Hello, Since I am facing something which look similar, I took liberty to explain my issue on this post.. Using LOGO ref6ED1 052-1MD08-0BA0 and HMI KPT400 6AV2 123-2DB03-0AX0 The Logo! I8 is connected to a 4-20mA input from an ultra-sonic sensor (powered with the LOGO! supply). This is used to regulate a motor speed depending on the product position. The HMI is used to select regul mode or not. I benched tested program and hardware. Every thing was working nicely. We then placed the equipment in the electrical cabinet on production and every time the ultra-sonic sensor is triggered, the network input which link the HMI and the Logo! change status randomly without any external action. We looked at possible EM interference but could not find anything. It is a bit puzzling as when we benched tested it we didn't ground anything and obviously now on production line all requirement have been followed...??? Thank you your help or suggestions. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/10/2020 11:19:56New subject after splitting |
|
2/10/2020 10:20 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33800 Rating: (4199)
|
Could it be that you have an overlap in the VM area? Could you upload the LOGO! program as a ZIP Archive? |
4/29/2020 1:54 PM | |
Joined: 1/7/2019 Last visit: 12/1/2020 Posts: 3 Rating: (0) |
Hi, Apologies for this long break.. Please find under attached the program. Thank you, Regards, JF AttachmentHF_LoopCtrl_Logo_saved20200422_1100.zip (187 Downloads) |
4/29/2020 3:18 PM | |
Joined: 1/7/2019 Last visit: 12/1/2020 Posts: 3 Rating: (0) |
Thank you. |
This contribution was helpful to1 thankful Users |
4/29/2020 3:23 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33800 Rating: (4199)
|
Hello JF_S, you're welcome ... In attachment a bit more Information. AttachmentLOGO! Bit, Byte, Word and DWord.pdf (271 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on