8/17/2020 9:46 AM | |
Posts: 21 Rating: (0) |
Dear Milos, I have problem with TCP/Ip connection inside Protocol suite (TAg Management). I just replaced complete unit of IPC477D, because the previous IPC477D was faulty. And for temporary I put laptop as HMI for panel operator. I created project "SaveAs" from Project Duplicator application, and copy past into new IPC. Here are what I did: 1. Checked IP address of new IPC follow the old one. 2. Checked AS ip address in TCP/IP parameter of new IPC. 3. Checked which port of ethernet connection that we use at new IPC. But still the icon status of AS inside "Tag Management" is "Disconnected". what are the other possibility the problem ? what should I do next ? Thank you in advance YanB ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/17/2020 13:02:57New subject after splitting Last edited by: YANB at: 08/18/2020 09:10:09 |
|
8/17/2020 1:13 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello YANB, you need to set the right logical device name for TCP/IP https://support.industry.siemens.com/cs/ww/en/view/12125202 Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
8/17/2020 9:37 PM | |
Posts: 21 Rating: (0) |
Hi Georg, I have open link given. Check on the new IPC, they are already the same parameter, here are the screenshot as attached. For info; I bought IPC477D, it comes with WinCC installed, I can check original IP address from Netpro, but I do not know what is the previous host name of the faulty IPC. that why i just put computer name on it. The architecture is simple, redundant S7400 with only have 1 HMI (IPC477D) which have Ethernet cable connected directly to CP CPU Rack0. Thank you and best regards YanB |
Last edited by: YANB at: 08/18/2020 09:01:58 |
|
8/18/2020 9:08 AM | |
Posts: 21 Rating: (0) |
Hi George, Do I need to do compile & download OS from Simatic Manager ? I see OS inside the S7400 (AS) project, please see the screenshot. Best Regards YanB |
8/18/2020 9:14 AM | |
Posts: 21 Rating: (0) |
Hi Georg, Here the connection parameter setting, basically it already inside, because I take the OS project from "Project Duplicator" and do SAVEAS Thank you YanB |
8/20/2020 7:14 AM | |
Posts: 21 Rating: (0) |
Hi Georg, Do you think, I need to re-download OS from project (simatic manager) which is in laptop now ? Here I attached system architecture. Mit freundlichen Grüßen und gesund bleiben YanB AttachmentMEG_system architecture.pdf (172 Downloads) |
Last edited by: YANB at: 08/20/2020 07:15:01 |
|
Follow us on