4/5/2018 3:43 PM | |
Posts: 9 Rating: (0) |
Hi, i am new to this siemens stuff and was looking to get Temperature data from a sensor we have, i added the data log into the program and it output data of sorts fine twice into different file names. i then tried to add more items for it to log and deleted the csv files from the location on the desktop as i thought maybe i was just seeing the same data. when i tried to log again it now just gives me the message 'No data log is found'. does anyone know how to fix this? *Edited text* there is no sd card so i am just using the memory. i turned the siemens off and back on and it let me write one csv file but now wont do another again. Thanks kev ------------------------------------------------------------------------------------------ AttachmentHeizung WAS2016047 einzel Wz 0.2.1 modified with data logging.zip (630 Downloads) |
Last edited by: Kevgray at: 4/5/2018 4:22:24 PMLast edited by: Jen_Moderator at: 4/6/2018 7:19:02 AMNew subject after splitting |
|
4/5/2018 4:23 PM | |
Posts: 9 Rating: (0) |
hi i have added the file and i am just writing to the module as i have no card. the Attachement is in my original post thanks |
4/6/2018 9:34 AM | |
Posts: 9 Rating: (0) |
Thanks all, i now seem to have data go that's a good start. My next question is that there is a temperature sensor and when it goes below the set point it starts the heating and visa versa when its too hot starts the cooling. but in my data i cannot see the actual temperature. Is that because i am not connecting my data log from the correct trigger or is this not even possible to monitor? TIA Kev attached is my modified program connecting to all data and a copy of the data i have from the program AttachmentHeizung with all data.zip (655 Downloads) |
Follow us on