12/10/2015 11:25 AM | |
Joined: 12/1/2015 Last visit: 3/27/2020 Posts: 3 Rating: (0) |
Dear bg2492 Thank you for your quick response. No the picture is at the center of the main screen and doesn't cover the object that is actually disappear.The object is a tank and it comes back on but half of it. In another screen for example when the window pop up,the background on the left goes gray and covers some measurement I/O field. Here is some examples in the photo. |
9/29/2016 4:29 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by gabbar is split to a separate thread with the subject Question marks appears instead of text in WinCC v7.3 runtime. Best regards |
Follow us on