11/28/2008 5:54 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Buon giorno, fete; I don't know if objects such as you are looking for exist in WinCC, beu here you will find the link to the WinCC basic manual (in Italian): Non so se gli oggetti come voi propongono sono disponibili, ma questi siano quei che vengano nell' Toolbar standard di WinCC. Qui è un link alla versione italiana della documentazione di base di WinCC http://support.automation.siemens.com/WW/view/en/15342782/0/it
6AV6392-1XA06-0AB0 4.1.1 The start screen of the Graphics Designer Introduction The Graphics Designer provides objects and tools for creating process pictures. Start the Graphics Designer from the navigation window of the WinCC Explorer. Layout of the Graphics Designer screen The Graphics Designer is designed according to the Windows standard. The Graphics Designer has a desktop, toolbar, menu bar, status bar and various palettes. When you open the Graphics Designer, the screen with the default settings appears. As standard, a blank picture is displayed (file format PDL). You can move the palettes and bars on the screen and arrange them as you like. The toolbars At "View", "Toolbars...", the following toolbars can be shown or hidden. In the default setting, all toolbars, except for the tags, are shown. • Objects: for inserting Standard Objects, Smart Objects, Windows Objects andControls. • Styles: for changing the line type and thickness, and fill patterns.. |
11/29/2008 10:52 PM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
Hello fefe, welcome to our Technical Forum. Great that you got a reply by Daniel. Hope it will be helpful. Please try to publish your postings in english language. It will be much easier for the community to follow up the discussion if we all try to speak the same language. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
12/1/2008 9:54 AM | |
Joined: 11/28/2008 Last visit: 8/7/2024 Posts: 2 Rating: (0) |
OK, EXCUSEME. THANKS YOU
|
Follow us on