2/16/2021 10:13 AM | |
Joined: 11/20/2018 Last visit: 2/25/2022 Posts: 29 Rating: (0) |
I have a PLC running a large press machine. It ran perfectly at the start and then it began to every so often it would go into error mode and stop. It was happening say once a month. Now it is happening more and more frequent on a daily basis now. It is holding up the production badly now so I need to sort it. I have looked through the error log and it seems to think one of my expansion modules is being unplugged during the cycle. However I have checked everything is plugged in correctly and unplugged and plugged everything in again. The PLC is in a large metal enclosure so is well protected. I have attached the most recent error log. It also states that the AQ board is losing voltage during the cycle. I am guessing these two errors are directly linked. Does this mean my plc / expansion modules are faulty? Is there any other checks I can do or anything else that could be causing these errors? Would greatly appreciate your feedback as I am at a lose end and don't want to buy new plc/expansion boards if it is not needed. AttachmentDiagnostics.txt (458 Downloads) |
2/16/2021 2:36 PM | |
Joined: 7/9/2015 Last visit: 5/6/2024 Posts: 3819 Rating: (554)
|
Hi, I would do a firmware update of PLC and your AQ Modul. If it´s 6ES7232-4HB32-0XB0 newest FW is V2.1.1 > you get it there: Firmware update for S7-1200 Analog Output SM 1232, 2AOFollowing changes: HW component Update without function change to improve module Electromagnetic Compatibility Regards, Towome |
|
|
Follow us on