9/5/2012 1:28 PM | |
Posts: 18 Rating: (1) |
Returned all existing S7-1211 PLC's back to Siemens, and got 1214 models in exchange |
10/5/2012 9:49 PM | |
Posts: 18 Rating: (1) |
hi buddies Siemens has released a new firmware that prevents error described in this post. Beware, the upgrade is not necessary for all the issued PLC's except for those that are on the list. I think it's best if your supplier check serial numbers Enter the following FTP-Adress into the Adress-line of your File explorer (don't use the Internet Explorer). ftp://audsupport:quoo4Ueg@ftp.sbs.de/S7-1200_Firmware_V3.0.2.zip Note: this download will be deleted automatically in 5 days. |
10/22/2012 10:37 AM | |
Joined: 8/3/2011 Last visit: 8/22/2024 Posts: 100 Rating: (7) |
Hi, Could You be so kind and provide this fw 3.0.2 download again...It is deleted now..Thanks a lot |