4/24/2013 3:33 PM | |
Posts: 5 Rating: (0) |
if anyone can help me to get an output higher than 1kHz i would be thankful. i'm attaching the file i used in s7 basic V10.5
AttachmentPULSE.zip (110 Downloads) |
4/25/2013 10:54 AM | |
Posts: 5 Rating: (0) |
Here the other program...the Hard trigger |
4/25/2013 12:15 PM | |
Posts: 5 Rating: (0) |
Hi, I need it to control a step-step motor (SANMOTION SH1603) with a driver bipolar that needs a PULSE to control the speed. That pulse that can vary between 0 Hz and 10 kHz. Im using Siemens S7 1200 with SIMATIC V10.5 Ive already tried following the steps ofhttp://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=38391227&caller=view but I couldnt get to make it, and also I couldnt use the file because its for V11 and I have V10.5 Dont you have any prorgram or bloc similar to control the motor or any configuration for an outlet pulse. You could find attached the program that Ive made. I look forward to hearing from you. Thanks, AttachmentPTO.zip (104 Downloads) |
Follow us on