5/19/2020 10:51 PM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating: (2) |
Hello I am trying to connect two LOGO!8 FS4 by addressing VB blocks. but the second LOGO! cannot read the VB blocks from the first one. Device 1: LOGO8 FS4 IP: 192.168.1.5 255.255.255.0 Gateway: 192.168.1.1 Device2: LOGO8 FS4 IP: 192.168.1.6 255.255.255.0 Gateway; 192.168.1.1 the second LOGO! can read Q(NI4) and I(NI5) from the first LOGO! but cannot read VB blocks NI1, NI2 and NI3 what's the problem?
AttachmentLOGO_Snap.zip (182 Downloads) |
5/20/2020 5:18 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33827 Rating: (4203)
|
The problem in your file is that you want to transmit the three signals (V1.0, V1.1 and V1.2) twice. Once from the 1st LOGO! to the 2nd LOGO !, whereby the 1st LOGO! works as a client. Then again from the 1st LOGO! to the 2nd LOGO !, whereby the 1st LOGO! works as a server. I corrected that and removed the unnecessary transfers.
Attachment1399-02-30---Network_Project_01_V2.zip (195 Downloads) |
This contribution was helpful to1 thankful Users |
5/20/2020 8:07 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33827 Rating: (4203)
|
The easiest way is per Drag & Drop.
AttachmentScreenshots.zip (200 Downloads) |
This contribution was helpful to1 thankful Users |
5/20/2020 8:13 AM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating: (2) |
|
Follow us on