6/30/2009 8:30 AM | |
Posts: 3609 Rating: (29) |
|
6/30/2009 8:43 AM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124)
|
Hi, I know the simulation programs "Simply Modbus TCP 1.3.4" (modbus client) and "mod_RSsim" (modbus server). If you use the ModbusTCP Wizard to configure the PARAM_DB, you needn't change the parameters in the DB manually after that. The wizard insert the necessary parameters. If you want to know the meaning of the parameters, go to UDT65 in the standard library/communication blocksand click "F1". In this online help you find the description. Or you open the manual of the ModbusTCP product, page 4-3. Here you find the description as well. To open theexample project: go to SIMATIC Manager -> Open -> tab "examples" -> button "Browse..." -> select the project "MB_PN_CPU" in EXAMPLES. Wüstenräuber |
Last edited by: Wuestenraeuber at: 6/30/2009 8:45 AM |
|
6/30/2009 1:05 PM | |
Posts: 6 Rating: (0) |
Hi Mr.Wüstenräuber, I am download mod_RSSim. I am test and comment. Thank you Diego |
7/1/2009 2:22 PM | |
Posts: 6 Rating: (0) |
Hi, property WRITE_READ run OK. When I am toggle, can read and write. but it is not useful for me. I am need that communication run alone. I haveput PLC S7 how server? Or I have declare two instance to FB102 and declare one transmision area and other reception area? I am attach my program. Very thank for your assistance is very important for me. Best regards. Diego Attachmentmb.zip (761 Downloads) |
7/2/2009 8:47 PM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124)
|
You're welcome. |
Follow us on