1/20/2012 9:45 AM | |
Posts: 30 Rating: (0) |
After i installed the latest update for WinCC 7.0 i'm facing som problems. 2012-01-20 09:30:51.341 - ccProjectMgr.exe ControlService failed for CCPackageMgr with error 1062: The service has not been started. 2012-01-20 09:30:52.279 - ccProjectMgr.exe ControlService:No progress made within the wait hint failed for CCNSInfo2Provider with error 6: The handle is invalid. 2012-01-20 09:30:52.294 - ccProjectMgr.exe ControlService failed for CCNSInfo2Provider with error 1062: The service has not been started. 2012-01-20 09:30:52.419 - ccProjectMgr.exe ControlService:No progress made within the wait hint failed for CCDeltaLoader with error 183: Cannot create a file when that file already exists. 2012-01-20 09:30:52.435 - ccProjectMgr.exe ControlService failed for CCDeltaLoader with error 1062: The service has not been started. 2012-01-20 09:33:50.984 - ccProjectMgr.exe CSingletonProject::AttachDatabases pICCDBManagement->AttachDatabase RT \\DKYIT-L-0001880\WinCC_Project_12001\12001RT.mdf on DKYIT-L-0001880 failed: 0x80004005 2012-01-20 09:34:05.797 - ccProjectMgr.exe StartService ss.dwCurrentState != SERVICE_RUNNING failed for CCNSInfo2Provider with error 183: Cannot create a file when that file already exists. HELP |
1/11/2013 3:41 PM | |
Posts: 35 Rating: (4) |
Same problem. Any solutions? |
8/5/2013 6:29 PM | |
Joined: 2/15/2009 Last visit: 1/31/2024 Posts: 12 Rating: (1) |
use Windows Server on ES, should work... |
Follow us on