8/6/2018 12:33 AM | |
Joined: 12/12/2008 Last visit: 4/18/2024 Posts: 69 Rating: (6) |
Hi, Staight to the case: There have been some earlier posts in this forum on screens and suggested 3D print LIDs for the IOT20x0. No offense to the creators, but lets face it; they are nor pretty or have sufficient functionality. This post is a request to Siemens to embrace an idea to start producing a LID for the IOT20x0 for the Nextion 2.4" screen. A low-cost ideal screen for the IOT: https://www.itead.cc/nextion-nx3224t024.html I have CNC`d a lid for PoC, and I think it could be really nice if Siemens would sell injection moulded LIDs, with 4 screws and some screw holes. (And chamfered edge down to the screen surface on the front) The panel only consumes 90mA@5V at max. Dimmable and "sleepable". It has mature software, Arduino lib as well as NPM lib + simple UART interface TX/RX for direct serial towards Node-Red for example. It is a good product for 14.11 EUR! BR Benjamin Kruger |
This contribution was helpful to3 thankful Users |
Follow us on