12/14/2020 12:42 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello daercole, this error can have some different reasons: 1. delete the dcf-files and re-create the Server package and rebooting the PC. see FAQ: https://support.industry.siemens.com/cs/de/en/view/109763043 2. An other problem was solved by installing a driver for the network card, 3. Sometimes it happens when changing IP-address while a project is open. Run Security Controler 4. If you have Windows 7, you can sometimes fix these errors by uisng a Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
12/14/2020 2:05 PM | |
Joined: 4/7/2012 Last visit: 9/20/2024 Posts: 115 Rating: (4) |
thank's for answering. I think your point 1 could be the soluction. BUT while I was waiting some answering helps, I did install Update 8 (of Wincc 7.0 SP3), and it seems that work. I keep this info when I will not have any more update to install. |
Follow us on