12/1/2020 12:34 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello Jorge KW, with the database of WinCC only Windows Authentication is used. see the Application example: https://support.industry.siemens.com/cs/ww/en/view/38132261
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
12/1/2020 2:40 PM | |
Posts: 80 Rating: (0) |
Thanks but I keep getting the error attached ("The login is from an untrusted domain"). So I think the problem is due to the fact that I am trying to connect from another machine. How can I configure this to allow connecting not only from local machine? Also, would it be possible to connect to it from an outside SW with a SQL Server Driver? Regards
|
Last edited by: Jorge KW at: 12/01/2020 15:00:40 |
|
12/8/2020 1:22 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello Jorge KW, if you get a message like "The login is from an untrusted domain", https://docs.microsoft.com/en-us/azure/active-directory-domain-services/tutorial-create-forest-trust
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on