10/30/2006 9:21 PM | |
Posts: 1275 Rating: (123)
|
I think so too! Siemens does have some amazing tools! If you have any further doubts, feel free to post! [:)] Best regards, Danielle |
10/31/2006 9:03 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
Hi guys It's worth mentioning that you can use Redundancy between to single-user projects. In this case neither WinCC computers are WinCC Servers so you should be able to use XP. This is based on the information in this FAQ Salma |
Last edited by: salma at: 10/31/2006 9:04 AM |
|
10/31/2006 11:43 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
Are you using the WinCC Redundancy Option ? If yes then this can be used with two single-user projects. In this case you do not need the WinCC Server Option OR W2003 Server. You can use XP Professional instead. |
Follow us on