4/22/2008 4:39 PM | |
Posts: 22 Rating: (0) |
Hello Molly, thanks for you response, you could be more explicit.. |
4/23/2008 10:49 AM | |
Joined: 4/21/2008 Last visit: 3/13/2024 Posts: 12 Rating: (2) |
Hi CJG, there are two method tointegrate simocode pro in the step7 system, 1.via GSD(general station describe) file,you can download the GSD file fromthe internet under http://www.ad.siemens.de/csi_d/gsd 2. integration of simocode pro as S7 slave via OM(object manager) simocode pro. the "OM simocode pro "software is included in the scope of delivery of the "simocode ES professional"software. during you intall the simocode ES professional, also select the "OM simocode pro" (make a tick mark). after install the software you can configurate simocode pro via OM .(see the attach). CJG, if you want to use the simocode es routing function , please select option 2 AttachmentSIMOCODE ES routing.zip (1060 Downloads) |
This contribution was helpful to4 thankful Users |
4/23/2008 4:01 PM | |
Posts: 22 Rating: (0) |
Thanks very much, their help and assistance is appreciated, Best regards, Have a a nice day, week, weekend, month, year... |
12/4/2013 12:06 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question splitted to how many simocode OM can be connected on the DP master bus? Best regards O_Moderator |
1/9/2014 12:38 PM | |
Posts: 467 Rating: (59)
|
in this FAQ you can find the informations for the question http://support.automation.siemens.com/WW/view/en/51445298 best regards LesPaul |
Follow us on