9/1/2016 6:51 AM | |
Posts: 92 Rating: (5) |
Hi There I want to run C axis rotary ( Spindle , 810 GA2 ) in my turnung machine . I set the MDs 3442-4612-5602 , bit 7 /3 - 5642 bit5-5722 bit4 But i have reference not reched alarm, after set "3442 modul value for rotary axis " and ... I have Limitet C axis and reference C rotary alarm, what you think about this problem? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/1/2016 11:40:46 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
9/13/2016 6:51 AM | |
Posts: 92 Rating: (5) |
Hi there I have 2 microswitch behinde of spindle , what mirrors Arm position front of my spindle . I have One Spindle Motor and also One spindle drive . please download all attechment file , because of zip files size , i cant Upload Whole details. AttachmentHeid.zip (245 Downloads) |
9/13/2016 7:20 AM | |
Posts: 92 Rating: (5) |
I have One key , on my MCP , Witch I attached in the Picture. With tern right , My Spindle rotate with 10RPM CW , and turn left , its rotate CCW With 10RPM Speed. But No chenge in my C axis degre , on monitor. All my drives is INDRAMAT, and my spindle drive also support Index.I try too set refpoint C axis , But I dont Know How calciulate it? AttachmentHaid 2.zip (209 Downloads) |
Last edited by: Sky Diver840 at: 9/13/2016 8:15:31 AM |
|
9/13/2016 8:41 AM | |
Posts: 92 Rating: (5) |
there is a quastion , how can we set the " axis assignment " and other parameters ,on rottary index axis? an aim, witch is feed by hydrolic system is a switch between spindle and C axis . If the arm is enable , gears become engaged witch is shown via microswitch 1 and if the arm is desabled , spindle become enable witch is shown via microswitch 2 . What I show In attached picture. AttachmentMD explanation.zip (248 Downloads) |
Last edited by: Sky Diver840 at: 9/13/2016 8:47:04 AM |
|
Follow us on