12/17/2009 1:34 PM | |
Joined: 10/7/2005 Last visit: 5/14/2024 Posts: 3005 Rating: (1048) |
Just to be clear, the "Profinet" port of the S7-1200 can (currently) only be used for PLC-PLC and PLC-HMI comms. AddingProfinet I/OController capability to the Ethernet port ofthe 1200 is planned for late 2010, but I don't know if any plans exists foraddition of Profinet I/O Device functionality (and it is in my humble oponion more likely that a DP Slave module comes out first for the 1200). As for "Profibus is yesterday", well let's just say that I woulddisagree with that assertion (and so does the market if the growth figures are anything to go by, more can found here: http://www.profibus.com/news-press/detail-view/article/node-growth-exceeds-expectations/). |
Cheers |
|
12/17/2009 2:00 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242) |
Yes, its still growing and still it is very reliable connection, but Siemens make a lot of effort to push Profinet into marked and its good standard for fast communications and real-time control. Profibus is relatively old standard and I think in a couple of years situation in marked will change completely. I set my bet for Profinet . |
Best regards, |
|
4/25/2011 12:47 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1426)
|
Hi, there is now an offitial delivery release for TIA V11:
|
Denilson Pegaia |
|
Follow us on