1/14/2013 6:52 AM | |
Posts: 12 Rating: (0) |
Hi All, May i have a question about the sample program below? /tf/WW/en/Posts/57715 I have download the program and it work fine for the frist time, and i able to download the logging result via webserver. problem is, when i power OFF and ON the PLC, then i follow the same sequence to start the data logging, i found that, the block is not allow to create a data file, and i was not able to log the data anymore, but then, it will work only when i go in to the webserver and delete the perious log data. so can you please advice on this issue? in the other hand, can you also please advice how the "Data Log Open" ; "Data Log Close" ; "Data Log New File" work on this program? Thanks. |
1/14/2013 11:02 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread S7-1200 data logging block Best regards O_Moderator |
Follow us on