10/6/2014 10:21 AM | |
Posts: 27 Rating: (0) |
Thank you Huggy. Well I made all the changes that the TIA asked for. I will try again. |
10/10/2014 8:53 PM | |
Posts: 27 Rating: (0) |
Thank you for your fast response. Yes. I enabled the web server, selected the directory and the web page and generated the blocks. It is a basic program. I can see the DB333 and DB334 in the system blocks. I am getting the attached response from the browsers. So it does not even reach the basic page of the web server. Although as I explained earlier, pinging the IP address from the command prompt window is getting 0% loss, i.e. connectivity is working and also going online is working. It is the web page that I cannot reach. AttachmentS7_1212_Browser.pdf (96 Downloads) |
10/10/2014 8:57 PM | |
Joined: 7/7/2010 Last visit: 4/18/2024 Posts: 14594 Rating: (2347)
|
Try typing http:// in front of those numbers.
|
science guy |
|
Follow us on