4/5/2012 7:20 AM | |
Joined: 8/31/2010 Last visit: 9/24/2024 Posts: 1521 Rating: (227) |
Hello pethkarashu, Do you have an empty SIMATIC Memory Card? Try this if it canmake your desired outcome. - Recovery from a lost password This is the standard method for Resetting to factory settings. |
Like it? Rate it! |
|
1/25/2013 8:21 AM | |
Joined: 8/31/2010 Last visit: 9/24/2024 Posts: 1521 Rating: (227) |
Hello RND, Before you download the contents to the PLC, you view the accessible devices and then as shown below double click the "Online & diagnostics" where you can determine the actual Firmware of the CPU. Now set the same firmware of the CPU (also the same MLFB);Make sure the IP address of the PG/PCis in the subnet of the PLCand then try to download, where you should be able to succeed. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
1/25/2013 10:24 PM | |
Joined: 8/31/2010 Last visit: 9/24/2024 Posts: 1521 Rating: (227) |
Hello RND, Operating System Update for SIMATIC S7-1200 CPU Firmware V3 - http://support.automation.siemens.com/WW/view/en/64789124 Have a look @ this entry, as it says v3.0.2 has a fix for it. |
Like it? Rate it! |
|
Follow us on