2/26/2016 9:53 AM | |
Posts: 8 Rating: (0) |
The CPU which i'm using is S7-1200 CPU 1212C (6ES7 212-1AE40-0XB0) firmware V4.1 and CM module CP 1243-1 (6GK7 243-1BX30-0XE0) firmware V2.0. |
2/26/2016 10:05 AM | |
Posts: 8 Rating: (0) |
Thx for replay. Can You which communication properties You are talkink abut, because i'm not sure if I understand You mean? |
12/19/2019 7:53 AM | |
Joined: 10/24/2012 Last visit: 6/1/2024 Posts: 310 Rating: (21) |
I know its an old post but according to the S7-1200 manual V4.3/2019, you can only read the status of RUN/STOP , ERROR, MAINT LEDs wit the LED block. Please read the chapter 9.7.3 of the attached link https://cache.industry.siemens.com/dl/files/129/109764129/att_974298/v1/s71200_system_manual_en-US_en-US.pdf |
Kashir Saeed. |
|
Follow us on