4/17/2016 7:24 AM |
|
Joined: 10/31/2014 Last visit: 3/1/2024 Posts: 58 Rating: (5) |
Hello, If my program is made in TIA V11. And i would like to take backup from TIA V13. is there any solution behind that? |
4/17/2016 8:40 AM | |
Posts: 153 Rating: (9) |
He want upload because he no have project how can he migrate project from TIA 11 to 13 |
4/17/2016 7:38 PM | |
Joined: 3/28/2015 Last visit: 5/4/2024 Posts: 721 Rating: (213) |
Hello, 1-Kindly have a look at this topic: 2-TIA V13 Licence can be used for TIA V11 or TIA V12 3-Download the trial Version of TIA V11 from Siemens Site. SIMATIC STEP 7 (TIA Portal) V11 SP2 TRIAL Download Hardware Support Packages (HSP) for WinCC (TIA Portal) V11 With TIA V13 licence,you can obtain the full version for TIA V11"Trial version". 4-You can install TIA V11 and TIA V13 together on the same PC. 5-Upload the program using TIA V11
|
Eng.Mohamed Ibrahim |
|
4/23/2016 8:27 PM | |
Joined: 7/19/2011 Last visit: 4/27/2024 Posts: 262 Rating: (5) |
Better to install v11 and do the rest as it seems there is no other solution for same. |
JAVED AKHTAR |
|
7/27/2016 9:03 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by 9583815919 is split to a separate thread with the subject Upload the program in TIA V11/V13. Best regards |
Follow us on