4/16/2008 1:58 PM | |
Posts: 125 Rating: (26) |
Hi Jeeps, maybe this FAQ helps you... http://support.automation.siemens.com/WW/view/de/2936808 Please make sure, you have explained the Function "Options -> Block Types.." in CFC - Editor for you changed FB, to take over the changes in all necassary places. Regards |
4/16/2008 5:00 PM | |
Posts: 218 Rating: (28) |
Hmmm, how come I never find those things. The explanation was what I needed. Will have to check what I did wrong then. :D thnx for the link. Jeebs |
7/22/2009 4:23 PM | |
Joined: 9/16/2008 Last visit: 8/29/2024 Posts: 56 Rating: (0) |
Hi Jeebs, You can assign S7_m_c attributes for IN Variable in FB. Assign in the IN parameter S7_m_c and make it true. In the FB properties also give the same. In the instance DB of the particular FB go to Special object properties and select WinCC attributes. Then Compile your OS. You will get the tag generated in your Win CC. Kindly go through the pictures attached with this. Hope this will help you. AttachmentWinCC.zip (476 Downloads) |
7/24/2009 4:25 PM | |
Posts: 28 Rating: (3) |
Did you activate "Operator Control and Monitoring" for the complete DB. Right click on DB -> Special Object Properties -> Operator Control and Monitoring.. |
7/24/2009 5:59 PM | |
Posts: 261 Rating: (42) |
Hi David, Yes it is also possible to use s7_m_c in a share DB. regards ddg |
7/27/2009 9:07 AM | |
Posts: 99 Rating: (7) |
It works also fine in a normal DB /tf/WW/en/Posts/30190#top Greetings ME |
Follow us on