5/19/2017 3:17 PM | |||
Posts: 9 Rating: (0) |
Hi experts, I am willing to connect my S7 CPU1518 (from X2 P1) to a WSN/PA link through modbus TCP I build MB_CLIENT and it fails with status 809B in the step7 documenation, 809B indicates "the ID of the local device in the connection description does not correspond to the CPU I can't figure out what is this about because it do not specify such id in my blocks ***UPDATE*** : I check the online help that indicates :
Then, I use : Local~PROFINET_interface_2~Port_1 : 73 to set in my TCON_IP-V4 interface id value but still, 809B error... see zip attachement for status in block thanks in advance AttachmentDocuments.zip (1844 Downloads) |
||
Last edited by: gillesbr at: 5/19/2017 3:27:12 PM |
|||
5/19/2017 4:18 PM | |
Posts: 3093 Rating: (323)
|
Hello Gilles, Regards, |
5/15/2018 12:02 PM | |
Joined: 12/28/2016 Last visit: 9/13/2024 Posts: 364 Rating: (6) |
I am having the same issue 809B |
With kind regards... |
|
8/10/2018 5:35 AM | |
Posts: 1 Rating: (2) |
enter 64 |
Follow us on