12/17/2008 7:40 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello To use with CPU via the Integrated PN Interface you must order: S7 OpenMODBUS/TCP PN PLC Single License MODBUS communication via the integrated PN-interface. In your case better use trial version of this (just to try with S7-400 PLC PN).Download (register before go to download). Please post your result here. I used thia with CPU317-2 PN/DP and this works but I can't find information about S7-400 PLC. regards |
This contribution was helpful to1 thankful Users |
12/18/2008 3:43 AM | |
Posts: 9 Rating: (0) |
Yes I realized that this driver will be released soon. THANK |
2/16/2009 7:53 AM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124)
|
Hi carestradas, I can give you a great information: The new version of "OpenModbusTCP PN CPU" is released. In this version the additional function codes 1, 2, 4, 5, 6 and 15 (conformance class 1) are supported and it is released for 400 PN CPUs as well. The current manual is downloadable here soon (if the date of change is newer than today ) and in this posting. Wüstenräuber AttachmentModbus TCP PN_CPU English.pdf (1931 Downloads) |
This contribution was helpful to1 thankful Users |
2/19/2009 4:54 PM | |
Posts: 9 Rating: (0) |
Ok Thank Let me check thisPDF manualand I hope tofind whatIm lookin for. |
Follow us on