6/16/2010 4:41 PM | |
Posts: 7 Rating: (0) |
Hi, I've managed to get comm's between my S71200 PLC and Metler Toledo weigh scales. The scales are set to send continous weight values, so I am only setup on the PLC side to receive from the weigh scale. Issue that I have is that post download or post my program run (runs for x cycles then stops) I have to start/stop PLC so as to get conitnuous data updates from my weighscales, i can get instantaneous weight but this is a does not change when scales change. I cycle PLC a couple of times and it operates as expected. Please see screen dump of attachment. Best Regards, Nicky. Attachmentrs232_.pdf (991 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on